MITSUBISHI ELECTRIC Changes for the Better
Russia

Make electrical equipment multi-functional by means of Mitsubishi air circuit breakers that are suitable for protection of the main circuit

Air circuit breakers have many advantages, among them adding higher reliability during switching. They can be used to extend the area of selective coordination trough expansion of the rated short-time withstand current, for use in main circuit ports.

Air Circuit Breakers (ACB) AE-SW

This kind of breaker is used as the main power breaker of the supply such as buildings, factories and ships etc. and satisfy the various needs.