FOR IMMEDIATE RELEASE No. 3168

Mitsubishi Electric's New "REESA" Small, Low-cost Array Antenna Achieves High-precision Beam Scanning

PDF Version

TOKYO, February 6, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today its development of the REESA (Rotational Element Electronically Scanned Array) antenna, a small, low-cost array antenna that achieves high-precision beam scanning by electronically rotating antenna elements individually. The REESA antenna is suitable for airport radar systems, mobile satellite communication systems and possible new applications such as microwave-based industrial heating and mounting on drones for long-distance data transmission. Commercialization of the product is targeted at 2020.

Key Features

1)
Rotates antenna elements individually for precise phasing and beam scanning
- Controls phase by rotating circularly polarized antenna elements individually by motors
- Realizes high-precision beam scanning by controlling phase in approx. two-degree increments
- Smaller and les expensive than conventional mechanically driven parabola antennas and active electronically scanned arrays (AESAs).
2)
Achieves high efficiency and low power consumption
- Uses a hollow waveguide for the antenna feed to achieve high efficiency of 85 percent in 12 GHz band

Note that the releases are accurate at the time of publication but may be subject to change without notice.