Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3301
TOKYO, September 10, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today its coming launch of a low-cost half-bridge driver high-voltage (600V) integrated circuit (HVIC) that achieves low pricing and high noise resistance by emphasizing basic functions. The new HVIC, designed for circuits that drive power semiconductors in low capacity inverter systems, is expected to lower the power consumption of white goods, electric bikes and industrial equipment. Sales will begin on October 18, 2019.
New low-cost 600V HVIC (M81776FP)
HVICs that drive power semiconductors in inverter systems are in increasing demand for use in motor control systems that help to save energy and improve the performance of consumer products and industrial equipment. Mitsubishi Electric HVICs combine highly reliability, cost effectiveness and compact designs.
Product | Model | Specification | Release |
---|---|---|---|
600V HVIC | M81776FP | 600V / -0.35A, +0.2A | Oct 18, 2019 |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.