Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
FOR IMMEDIATE RELEASE No. 3175
Is expected to help reducing IoT device sizes and power consumption
TOKYO, February 14, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed the world's first wireless communication technology capable of automatic optimization using its Maisart* proprietary artificial intelligence (AI) and advanced digital technology to enhance both performance and capacity. In tests, the amplifier has been proven to achieve double the normal gain and improve power efficiency by 20 percentage points compared to conventional systems. Furthermore, the transmitter can use various wireless communication access-mode standards while transmitting up to three arbitrary operating frequency bands simultaneously on a single circuit. This novel technology, which incorporates Mitsubishi Electric's proprietary AI and all-digital technologies, is expected to significantly reduce the power consumption, improve the miniaturization and support the globalization of multiband IoT equipment for multiple communication standards and regulations.
* Mitsubishi Electric's AI creates the State-of-the-ART in Technology
Gain | Efficiency | Bands/standards | |
---|---|---|---|
New Technology | 15 dB | 55% | 3 |
Conventional Technology | 12 dB | 35% | 1 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.