Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3300
TOKYO, September 10, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will release the FR-E800 series power inverters, with a range of 44 new models, from December 9. The new series, with safety functionality meeting IEC 61508 standards, supports various networks such as CC-Link IE TSN, a next-generation open industrial network, and make manufacturing smarter in various fields by integrating the world's first*1 corrosive gas environment detection circuit*2 and the industry's first*1 AI-based diagnostic functions. From April 2020, Mitsubishi Electric will release successive new models with safety communication features such as safely-limited speed, similarly conforming to relevant IEC standards. The product range will be further expanded to a total of 120 models.
FR-E800 series
Specification | Type | Price | Development completion |
Sales target |
---|---|---|---|---|
Ethernet models (22 models) |
FR-E820-0.1KE to 7.5KE, 9 models | Contact our customer support |
December 9 | 850,000 units in FY 2021 |
FR-E840-0.4KE to 7.5KE, 7 models | ||||
FR-E860-0.75KE to 7.5KE, 6 models | ||||
Standard models (22 models) |
FR-E820-0.1K to 7.5K, 9 models |
|||
FR-E840-0.4K to 7.5K, 7 models |
||||
FR-E860-0.75K to 7.5K, 6 models |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.