Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3338
TOKYO, February 19, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that in late May it will begin sample sales of a new 10.4-inch XGA TFT-LCD module designed for use in harsh environments, including construction sites, heavy-duty vehicles, agricultural areas and industrial applications.
The new module will offer an unprecedented combination of advanced features, including high-resolution XGA (1,024 × 768 pixels), super-wide 176-degree horizontal/vertical viewing angles and high luminosity of 1,300 cd/m2. It will also boast a number of attributes for which market demands are increasing, such as a high contrast ratio of 1,000:1, a versatile storage-temperature range of -40 to +80 degrees Celsius and high resistance to vibration.
Sample sales will commence on May 29 through Mitsubishi Electric offices worldwide.
Mitsubishi Electric's AA104XN11 color TFT-LCD module
Product | Size | Resolution | Model | LED driver | Sample Shipments |
---|---|---|---|---|---|
TFT-LCD Module | 10.4-inch | XGA | AA104XN01 | Yes | May 29, 2020 |
AA104XN11 | No |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.