Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3341
TOKYO, February 27, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its subsidiary Mitsubishi Elevator India Private Limited (IMEC) has secured a major order from the "All India Institute of Medical Science (AIIMS), Bilaspur, Himachal Pradesh." The order consists of a total of 64 elevators, including 48 of a model that is exclusive to the Indian market, at this Indian government-owned medical facility, which houses a hospital and a national medical institute. By means of these high quality elevators and services, Mitsubishi Electric aims to provide the safe and reliable vertical transportation required by medical facilities.
Image of Mitsubishi Elevator "NEXIEZ-LITE MRL"
Rendering of AIIMS
Of the 64 elevators, 48 are "NEXIEZ-LITE MRL," models designed exclusively for the Indian market which were released in April 2019 and are manufactured by IMEC. They are equipped with specific functionality required in India such as automatic emergency landing devices, which operate in the case of a power failure, as standard.
Product | NEXIEZ-LITE MRL | NEXIEZ-MRL |
---|---|---|
Units | 48 units | 16 units |
Specification | 13~15 persons 60 m/min. | 21 persons 60 m/min. |
Supplier | Mitsubishi Elevator India Private Limited (India) | Mitsubishi Elevator Asia Co., Ltd. (Thailand) |
Schedule | Will ship from March 2020 |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.