Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3367
TOKYO, August 25, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of its LV100-type T-series insulated-gate bipolar transistor (IGBT) module for industrial uses. The LV100 package, which achieves high versatility and high current density, has been used widely in railway and electric power applications and now has been adapted for industrial uses. It is expected to help reduce the size and power loss of power converters, specifically inverters used for renewable energy applications such as photovoltaic and wind-power generation, and also high-capacity motor drives. Sales will start this September.
LV100-type T-series IGBT module for industrial use
Product | Model | Rating | Release date |
---|---|---|---|
LV100-type T-series IGBT module for industrial use |
CM800DW-24T | 1200V / 800A | September 2020 |
CM1200DW-24T | 1200V / 1200A | ||
CM800DW-34T | 1700V / 800A | ||
CM800DW-34TA5 | 1700V / 800A | ||
CM1200DW-34T | 1700V / 1200A |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.