Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3727
Presentation ceremony on September 2, 2024
Fences being installed off Takana Beach, Iriomote Island
TOKYO, September 3, 2024 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has built undersea conservation fences off Iriomote Island, Okinawa Prefecture, to protect tape seagrass, a Category II vulnerable species on the Ministry of the Environment's Red List, and donated the fences to the town of Taketomi in Yaeyama County, Okinawa Prefecture, which administers the island, during a ceremony on September 2.
In Japan, Tape seagrass, a species of the Hydrocharitaceae family that grows to about one meter in length, exists in colonies found only in Yaeyama Islands, of which Iriomote is the largest and most important habitat. The Ministry of the Environment's Red List quantifies assesses the risk of extinction for each species of wildlife living in Japan. Seagrasses, seaweeds, salt marshes and mangrove forests in coastal and marine ecosystems are major absorbers of so-called blue carbon, which is stored in their biomass and in the soil beneath them.
Through initiatives in diverse fields, Mitsubishi Electric is committed to reducing carbon dioxide emissions, a major contributor to climate change. Through field surveys of blue-carbon ecosystems, the company has confirmed that tape seagrass serves as a spawning and breeding ground for marine life, and also absorbs and fixes carbon dioxide from the atmosphere. As such, the species makes "nature-positive" contributions by not only reducing environmental damage, but also by enhancing biodiversity, improving ecosystem health, and supporting the sustainable use of natural resources. However, the species is now threatened with extinction, including around Iriomote, a World Natural Heritage Site, due to factors such as consumption by green sea turtles, which inhabit coastal areas in tropical and subtropical regions of the world and feed primarily on seaweed and seagrass like eelgrass, and are themselves classified as a Category II vulnerable species.
Tape seagrass with leaves shortened due to consumption by green sea turtles
Recognizing the urgent need for action, Mitsubishi Electric built protective fences around the tape seagrass beds off Takana Beach covering some 440 square meters. It is hoped that the fences will enable the remaining tape seagrass to recover to the point where it no longer needs protection, allowing green sea turtles to feed on it naturally, thereby supporting biodiversity as well as the absorption and fixation of carbon dioxide.
Going forward, Mitsubishi Electric will work with Taketomi town to explore additional measures, such as protection strategies that incorporate the use of light and sound, and calculating the amount of carbon dioxide fixed in blue-carbon ecosystems. Through such efforts, the company aims to restore the original ecological balance of the local marine ecosystem and make further nature-positive contributions on a larger scale.
Note that the press releases are accurate at the time of publication but may be subject to change without notice.