Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3445
TOKYO, October 21, 2021 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping samples of its 100Gbps (53Gbaud) four-level pulse-amplitude modulation (PAM4) electro-absorption modulator (EML) laser diode chip for coarse wavelength division multiplexing (CWDM) on November 1. The semiconductor diode is expected to be applied in sets of four EML chips as a light source in optical transceivers for 400Gbps optical fiber communication in data centers. Thanks to the new EML's operability in a wider range of temperatures, it will help to lower the power consumption and costs of optical transceivers by eliminating the need for conventional temperature-control units.
Product | Model | Wavelength | Temperature range | Shipment date |
---|---|---|---|---|
Wider-temperature-range CWDM 100Gbps (53Gbaud PAM4) EML chip |
ML7CP70 | 1271,1291, 1311 and 1331 nm |
5 to 85°C | November 1, 2021 |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.