Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3480
TOKYO, January 17, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a prototype of the world's smallest* antenna for high-precision satellite-based positioning in four frequency bands used by the world's main satellite-positioning systems and positioning-augmentation services.** The highly compact antenna, which is expected to be installed in diverse vehicles and even drones, will accelerate high-precision satellite-based positioning for autonomous driving and many other applications.
Prototype of compact antenna for satellite-positioning devices
Examples of satellite-positioning applications
Going forward, Mitsubishi Electric will research practical applications by evaluating the prototype's positioning precision in outdoor trials.
New antenna | Company A's | Company B's | Company C's | ||
---|---|---|---|---|---|
Size (including case) |
Horizontal surface | 59 mm x 59 mm | 140 mm x 140 mm | 160 mm diameter | 76 mm diameter |
Height | 33 mm | 62 mm | 60 mm | 35 mm |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.