Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3501
TOKYO, March 23, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its U.S. subsidiary Mitsubishi Electric Power Products, Inc. (MEPPI) has received a contract from Holtec International (Holtec) to expedite the design engineering of the digital instrumentation and control systems (I&C) for Holtec's SMR-160 small modular reactor which is a next generation small reactor with superior safety and reliability levels, featuring a natural cooling ability in case of any accidents.
MELTAC Nplus S digital safety I&C controller for SMR-160
Mitsubishi Electric and Holtec began developing preliminary designs for the SMR-160's I&C under an agreement signed in 2016 and will now accelerate these activities. Holtec, which aims to secure a SMR-160 construction license in 2025, is now considering deployment of a demonstration reactor.
In December 2020, Holtec was selected as an awardee by the U.S. Department of Energy Advanced Reactor Demonstration Program (ARDP) to design, engineer and license development of the SMR-160. Pursuant to the ARDP selection, Holtec issued the purchase order to Mitsubishi Electric to develop a control-room simulator that will be used to verify I&C design and review operation.
Holtec selected Mitsubishi Electric's MELTAC© controls for the SMR-160 design based on the company's long experience with nuclear power plant controls. In 2018, Mitsubishi Electric's MELTAC Nplus S safety control platform was favorably evaluated for use in U.S. nuclear power plants by the U.S. Nuclear Regulatory Commission.
Note that the press releases are accurate at the time of publication but may be subject to change without notice.