Файлы «cookie» помогают нам адаптировать сайт в соответствии с вашими потребностями, такими как язык или сфера интересов. Пожалуйста, подтвердите, что вы согласны на использование нами файлов «cookie».
News Releases
FOR IMMEDIATE RELEASE No. 3564
SLIMDIP-Z
TOKYO, December 13, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its new SLIMDIP-Z power semiconductor module, featuring an extra-high 30A rated current for use in inverter systems of home appliances, will be released in February 2023. The compact module will enable the SLIMDIP™ series to meet a wider range of power and size needs for inverter units, specifically by simplifying and downsizing systems for multifunctional and sophisticated products such as air conditioners, washing machines and refrigerators.
The demand is growing for power semiconductors capable of efficiently converting electric power to help realize a low-carbon world. In 1997, Mitsubishi Electric commercialized its first DIPIPM™ as a high-performance intelligent power module with a transfer-mold structure incorporating a switching device and a control IC to drive and protect the switching element. Since then, DIPIPMs have been widely adapted for use in large appliances and inverters for industrial motors, contributing to the downsizing and energy-efficiency of inverter boards.
Note that the press releases are accurate at the time of publication but may be subject to change without notice.